CPU3: failed to come online

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CPU3: failed to come online

1,640 Views
shalanyang
Contributor II

                    CPU3: failed to come online

we are useing IMX6QP for Auto Meter,we encounter the problen CPU3 can not bring up,the message is such as,please help me:

0.001] U-Boot 2015.04-g20acebff-dirty (Dec 21 2017 - 11:06:52)

[ 0.007] Board: MX6Q-PARIS3 revA
[ 0.011] I2C: ready
[ 0.013] DRAM: 2 GiB
MMC: FSL_SDHC: 0
[ 0.133] No MMC card found
[ 0.136] In: serial
[ 0.138] Out: serial
[ 0.140] Err: serial
[ 0.151] Normal Boot
[ 0.153] Hit any key to stop autoboot: 0
Loading Kernel Image ... OK
[ 0.260]
[ 0.261] Starting kernel ...

[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Initializing cgroup subsys cpuset
[ 0.000000] Initializing cgroup subsys cpu
[ 0.000000] Initializing cgroup subsys cpuacct
[ 0.000000] Linux version 4.1.15 (yangxiuliang@yxl-HP-Elite) (gcc version 5.2.0 (GCC) ) #1 SMP PREEMPT Thu Dec 21 11:09:33 CST 2017
[ 0.000000] CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine model: Freescale i.MX6 Quad/Solo SABRE Automotive Board
[ 0.000000] [MPU_MEMALLOC]:(func:mpu_reserve_memory)ipu phys=0x76800000
[ 0.000000] [MPU_MEMALLOC]:(func:mpu_reserve_memory)vpu phys=0x70400000
[ 0.000000] Reserved memory: created CMA memory pool at 0x48000000, size 320 MiB
[ 0.000000] Reserved memory: initialized node linux,cma, compatible id shared-dma-pool
[ 0.000000] Memory policy: Data cache writealloc
[ 0.000000] On node 0 totalpages: 459520
[ 0.000000] free_area_init_node: node 0, pgdat 405a0b00, node_mem_map bed57000
[ 0.000000] Normal zone: 4608 pages used for memmap
[ 0.000000] Normal zone: 0 pages reserved
[ 0.000000] Normal zone: 459520 pages, LIFO batch:31
[ 0.000000] PERCPU: Embedded 11 pages/cpu @bed09000 s16000 r8192 d20864 u45056
[ 0.000000] pcpu-alloc: s16000 r8192 d20864 u45056 alloc=11*4096
[ 0.000000] pcpu-alloc: [0] 0 [0] 1 [0] 2 [0] 3
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 454912
[ 0.000000] Kernel command line: vmalloc=800M bootmode=0 submode=0 console=ttymxc0,115200 androidboot.console=ttymxc0 init=/init arm_freq=800 lpj=7905280
[ 0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.000000] Dentry cache hash table entries: 262144 (order: 8, 1048576 bytes)
[ 0.000000] Inode-cache hash table entries: 131072 (order: 7, 524288 bytes)
[ 0.000000] Memory: 1484576K/1838080K available (4383K kernel code, 174K rwdata, 780K rodata, 396K init, 305K bss, 25824K reserved, 327680K cma-reserved, 0K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[ 0.000000] vmalloc : 0xc0800000 - 0xff000000 (1000 MB)
[ 0.000000] lowmem : 0x40000000 - 0xc0000000 (2048 MB)
[ 0.000000] pkmap : 0x3fe00000 - 0x40000000 ( 2 MB)
[ 0.000000] modules : 0x3f000000 - 0x3fe00000 ( 14 MB)
[ 0.000000] .text : 0x40008000 - 0x40512fec (5164 kB)
[ 0.000000] .init : 0x40513000 - 0x40576000 ( 396 kB)
[ 0.000000] .data : 0x40576000 - 0x405a19e0 ( 175 kB)
[ 0.000000] .bss : 0x405a4000 - 0x405f05b8 ( 306 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] Additional per-CPU info printed with stalls.
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] L2C-310 erratum 769419 enabled
[ 0.000000] L2C-310 enabling early BRESP for Cortex-A9
[ 0.000000] L2C-310 full line of zeros enabled for Cortex-A9
[ 0.000000] L2C-310 ID prefetch enabled, offset 16 lines
[ 0.000000] L2C-310 dynamic clock gating enabled, standby mode enabled
[ 0.000000] L2C-310 cache controller enabled, 16 ways, 1024 kB
[ 0.000000] L2C-310: CACHE_ID 0x410000c8, AUX_CTRL 0x76070001
[ 0.000000] mxc_clocksource_init 3000000
[ 0.000000] Switching to timer-based delay loop, resolution 333ns
[ 0.000007] sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 715827882841ns
[ 0.000027] clocksource mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns
[ 0.001041] Console: colour dummy device 80x30
[ 0.001061] Calibrating delay loop (skipped) preset value.. 1581.05 BogoMIPS (lpj=7905280)
[ 0.001078] pid_max: default: 32768 minimum: 301
[ 0.001191] Mount-cache hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.001205] Mountpoint-cache hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.001924] Initializing cgroup subsys blkio
[ 0.001943] Initializing cgroup subsys memory
[ 0.001981] Initializing cgroup subsys devices
[ 0.001998] Initializing cgroup subsys freezer
[ 0.002013] Initializing cgroup subsys perf_event
[ 0.002040] CPU: Testing write buffer coherency: ok
[ 0.002367] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[ 0.002443] Setting up static identity map for 0x10008280 - 0x100082d8
[ 0.080298] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[ 0.100271] CPU2: thread -1, cpu 2, socket 0, mpidr 80000002
[ 0.342507] Unable to handle kernel paging request at virtual address dff347bc
[ 0.342646] Unable to handle kernel NULL pointer dereference at virtual address 000001bf
[ 0.342711] Unable to handle kernel paging request at virtual address e63066eb
[ 0.342775] Unable to handle kernel paging request at virtual address a87101e4
[ 0.342841] Unable to handle kernel paging request at virtual address a87101e4
[ 0.342908] Unable to handle kernel paging request at virtual address a87101e4
[ 0.342971] Unable to handle kernel paging request at virtual address a87101e4
[ 0.343033] Unable to handle kernel paging request at virtual address a87101e4
[ 0.343099] Unable to handle kernel paging request at virtual address a87101e4
[ 0.343166] Unable to handle kernel paging request at virtual address a87101e4
[ 0.343228] Unable to handle kernel paging request at virtual address a87101e4
[ 0.343291] Unable to handle kernel paging request at virtual address a87101e4
[ 0.343358] Unable to handle kernel paging request at virtual address a87101e4
[ 0.343425] Unable to handle kernel paging request at virtual address a87101e4
[ 0.343488] Unable to handle kernel paging request at virtual address a87101e4
[ 0.343552] Unable to handle kernel paging request at virtual address a87101e4
[ 0.343618] Unable to handle kernel paging request at virtual address a87101e4
[ 0.343685] Unable to handle kernel paging request at virtual address a87101e4
[ 0.343746] Unable to handle kernel paging request at virtual address a87101e4
[ 0.343809] Unable to handle kernel paging request at virtual address a87101e4
[ 0.343876] Unable to handle kernel paging request at virtual address a87101e4
[ 0.343943] Unable to handle kernel paging request at virtual address a87101e4
[ 0.344004] Unable to handle kernel paging request at virtual address a87101e4
[ 0.344058] pgd = f49aa480
[ 0.344248] [a87101e4] *pgd=66b6e2f4, *pte=eb3c1c56, *ppte=3c8820bc
[ 0.344323] Internal error: Oops - BUG: 5 [#1] PREEMPT SMP ARM
[ 0.345580] Unable to handle kernel paging request at virtual address efbf00df
[ 0.347329] pgd = 696cbdd9
[ 0.347457] [efbf00df] *pgd=7b7df7f7(bad)
[ 1.119652] CPU3: failed to come online
[ 1.119688] Brought up 3 CPUs
[ 1.119703] SMP: Total of 3 processors activated (4743.16 BogoMIPS).
[ 1.119713] CPU: All CPU(s) started in SVC mode.
[ 1.131616] VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
[ 1.131998] clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 1.153388] pinctrl core: initialized pinctrl subsystem
[ 1.154507] NET: Registered protocol family 16
[ 1.164948] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 1.165857] mxc_arch_reset_init: failed to get wdog clock
[ 1.165872] CPU identified as i.MX6QP, silicon rev 1.0
[ 1.193232] hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
[ 1.193246] hw-breakpoint: maximum watchpoint size is 4 bytes.
[ 1.194229] imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
[ 1.195565] imx-gpc 20dc000.gpc: no fsl,ldo-bypass found!
[ 1.206449] mxs-dma 110000.dma-apbh: initialized
[ 1.220419] SCSI subsystem initialized
[ 1.220763] usbcore: registered new interface driver usbfs
[ 1.220845] usbcore: registered new interface driver hub
[ 1.220992] usbcore: registered new device driver usb
[ 1.221196] 2000000.aips-bus:usbphy_nop1 supply vcc not found, using dummy regulator
[ 1.221348] 2000000.aips-bus:usbphy_nop2 supply vcc not found, using dummy regulator
[ 1.222444] imx-i2c 21a8000.i2c: <i2c_imx_probe>
[ 1.222917] i2c i2c-2: IMX I2C adapter registered
[ 1.222938] i2c i2c-2: can't use DMA
[ 1.223079] Linux video capture interface: v2.00
[ 1.223135] pps_core: LinuxPPS API ver. 1 registered
[ 1.223145] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <[email protected]>
[ 1.223174] PTP clock support registered
[ 1.239721] imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
[ 1.242481] *** ipu_iauto_alloc_init: ipu_iauto_alloc_zone phys=0x76800000, virt=0xC1000000
[ 1.259722] imx-ipuv3 2800000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
[ 1.261536] Galcore version 5.0.11.41671
[ 1.642158] Switched to clocksource mxc_timer1
[ 1.645794] NET: Registered protocol family 2
[ 1.646481] TCP established hash table entries: 16384 (order: 4, 65536 bytes)
[ 1.646638] TCP bind hash table entries: 16384 (order: 5, 131072 bytes)
[ 1.646889] TCP: Hash tables configured (established 16384 bind 16384)
[ 1.647033] UDP hash table entries: 1024 (order: 3, 32768 bytes)
[ 1.647103] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes)
[ 1.647362] NET: Registered protocol family 1
[ 1.647685] Unpacking initramfs...
[ 1.707568] Freeing initrd memory: 764K (40e00000 - 40ebf000)
[ 1.707945] CPU PMU: Failed to parse /soc/pmu/interrupt-affinity[0]
[ 1.708016] hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available
[ 1.709732] Bus freq driver module loaded
[ 1.710962] futex hash table entries: 1024 (order: 4, 65536 bytes)
[ 1.720665] io scheduler noop registered
[ 1.720680] io scheduler deadline registered
[ 1.720875] io scheduler cfq registered (default)
[ 1.721344] imx-weim 21b8000.weim: Driver registered.
[ 1.721866] ldb 2000000.aips-bus:ldb@020e0008: split mode
[ 1.722227] ldb 2000000.aips-bus:ldb@020e0008: split mode or dual mode, ignoring second output
[ 1.723140] mxc_sdc_fb fb@0: registered mxc display driver ldb
[ 1.762232] imx-ipuv3 2800000.ipu: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)
[ 1.839617] Console: switching to colour frame buffer device 240x45
[ 1.931878] imx-sdma 20ec000.sdma: no iram assigned, using external mem
[ 1.933725] imx-sdma 20ec000.sdma: failed to get firmware from device tree
[ 1.937040] imx-sdma 20ec000.sdma: initialized
[ 1.937906] 2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 22, base_baud = 5000000) is a IMX
[ 2.899066] console [ttymxc0] enabled
[ 2.905030] PDRD call pdrd_proc_init() --start
[ 2.909760] PDRD create proc file: pdrd_switch
[ 2.914505] PDRD call pdrd_proc_init() --end
[ 2.919509] [drm] Initialized drm 1.1.0 20060810
[ 2.924630] [drm] Initialized vivante 1.0.0 20120216 on minor 0
[ 2.931804] spi_imx 2018000.ecspi: probed
[ 2.936897] usbcore: registered new interface driver asix
[ 2.942406] usbcore: registered new interface driver ax88179_178a
[ 2.948857] usbcore: registered new interface driver usb-storage
[ 2.954960] usbcore: registered new interface driver usb_ehset_test
[ 2.962285] snvs_rtc 20cc000.snvs:snvs-rtc-lp: rtc core: registered 20cc000.snvs:snvs-r as rtc0
[ 2.971129] i2c /dev entries driver
[ 3.032963] mxc_v4l2_output v4l2_out: V4L2 device registered as video16
[ 3.039735] mxc_v4l2_output v4l2_out: V4L2 device registered as video17
[ 3.047663] sdhci: Secure Digital Host Controller Interface driver
[ 3.053888] sdhci: Copyright(c) Pierre Ossman
[ 3.058258] sdhci-pltfm: SDHCI platform and OF driver helper
[ 3.064865] /soc/aips-bus@02100000/usdhc@0219c000: voltage-ranges unspecified
[ 3.072043] sdhci-esdhc-imx 219c000.usdhc: Got CD GPIO
[ 3.078233] sdhci-esdhc-imx 219c000.usdhc: No vmmc regulator found
[ 3.084468] sdhci-esdhc-imx 219c000.usdhc: No vqmmc regulator found
[ 3.132359] mmc0: SDHCI controller on 219c000.usdhc [219c000.usdhc] using ADMA
[ 3.144913] mxc_vpu 2040000.vpu_fsl: VPU initialized
[ 3.151369] *** vpu_iauto_alloc_init: vpu_iauto_alloc_zone phys=0x70400000, virt=0xCB000000
[ 3.164364] mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
[ 3.176615] ashmem: initialized
[ 3.184398] NET: Registered protocol family 17
[ 3.199123] snvs_rtc 20cc000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01 00:00:00 UTC (0)
[ 3.222293] usb_otg_vbus: disabling
[ 3.225825] usb_h1_vbus: disabling
[ 3.230314] Freeing unused kernel memory: 396K (40513000 - 40576000)
[ 3.239439] (II) init: command 'loglevel' r=0
[ 3.243937] (II) init: command 'write' r=0
[ 3.248143] (II) init: command 'write' r=0
[ 3.249316] mmc0: MAN_BKOPS_EN bit is not set
[ 3.256668] (!!) init: starting 'ueventd'
[ 3.260989] (II) init: command 'start' r=0
[ 3.267727] mmc0: new DDR MMC card at address 0001
[ 3.282684] mmcblk0: mmc0:0001 MMC08G 7.25 GiB
[ 3.287470] mmcblk0boot0: mmc0:0001 MMC08G partition 1 8.00 MiB
[ 3.293587] mmcblk0boot1: mmc0:0001 MMC08G partition 2 8.00 MiB
[ 3.299742] mmcblk0rpmb: mmc0:0001 MMC08G partition 3 128 KiB
[ 3.306421] mmcblk0: p1 p2 p3
[ 3.348706] EXT4-fs (mmcblk0p1): recovery complete
[ 3.353546] EXT4-fs (mmcblk0p1): mounted filesystem with ordered data mode. Opts: nodelalloc,journal_checksum
[ 3.363524] (II) init: command 'mount' r=0
[ 3.367653] (!!) init: processing action 0x1d782d8 (early-init)
[ 3.373638] (EE) init: command 'insmod /lib/modules/softdog.ko', r=-1
[ 3.380096] (!!) init: processing action 0x1d785f8 (wait_for_coldboot_done)
[ 3.387085] (II) init: wait for /dev/.coldboot_done
[ 3.391991] (II) init: command 'wait_for_coldboot_done' r=0
[ 3.397596] (!!) init: processing action 0x1d78640 (property_init)
[ 3.403803] (II) init: property init
[ 3.407696] (II) init: command 'property_init' r=0
[ 3.412526] (!!) init: processing action 0x1d78688 (console_init)
[ 3.418829] (II) init: command 'console_init' r=0
[ 3.423576] (!!) init: processing action 0x1d786d0 (set_init_properties)
[ 3.430396] (II) init: command 'set_init_properties' r=0
[ 3.435742] (!!) init: processing action 0x1d76f60 (init)
[ 3.441162] (II) init: command 'sysclktz' r=0
[ 3.445548] (II) init: command 'export' r=0
[ 3.449740] (II) init: command 'export' r=0
[ 3.453948] (II) init: command 'export' r=0
[ 3.458147] (II) init: command 'export' r=0
[ 3.462366] (II) init: command 'export' r=0
[ 3.466565] (II) init: command 'export' r=0
[ 3.470762] (II) init: command 'export' r=0
[ 3.474979] (II) init: command 'export' r=0
[ 3.479178] (II) init: command 'export' r=0
[ 3.483393] (II) init: command 'export' r=0
[ 3.487616] (II) init: command 'symlink' r=0
[ 3.491917] (II) init: command 'symlink' r=0
[ 3.496249] (II) init: command 'mkdir' r=0
[ 3.500375] (II) init: command 'mkdir' r=0
[ 3.504527] (II) init: command 'mkdir' r=0
[ 3.508732] (II) init: command 'mount' r=0
[ 3.512900] (II) init: command 'mkdir' r=0
[ 3.517091] (II) init: command 'mount' r=0
[ 3.521204] (!!) init: processing action 0x1d78328 (init)
[ 3.526640] (II) init: command 'export' r=0
[ 3.530840] (II) init: command 'export' r=0
[ 3.535055] (!!) init: processing action 0x1d783a8 (fs)
[ 3.540307] (II) init: command 'symlink' r=0
[ 3.544636] (II) init: command 'symlink' r=0
[ 3.548939] (II) init: command 'symlink' r=0
[ 3.553260] (II) init: command 'symlink' r=0
[ 3.557562] (II) init: command 'symlink' r=0
[ 3.561864] (II) init: command 'symlink' r=0
[ 3.566201] (II) init: command 'symlink' r=0
[ 3.570487] (!!) init: processing action 0x1d78718 (property_service_init)
[ 3.586282] (EE) init: Unable to open persistent property directory /var/property errno: 2
[ 3.594689] (II) init: Created socket '/dev/socket/property_service' with mode '666', user '0', group '0'
[ 3.604300] (II) init: command 'property_service_init' r=0
[ 3.609802] (!!) init: processing action 0x1d78760 (signal_init)
[ 3.615876] (II) init: command 'signal_init' r=0
[ 3.620511] (!!) init: processing action 0x1d772a8 (post-fs)
[ 3.626222] (II) init: command 'mount' r=0
[ 3.630329] (II) init: command 'class_start' r=0
[ 3.634982] (!!) init: processing action 0x1d773e8 (boot)
[ 3.640497] (II) init: command 'write' r=0
[ 3.644646] (!!) init: starting 'hotplug_event'
[ 3.649535] (!!) init: starting 'mount_usb'
[ 3.654091] (II) init: command 'class_start' r=0
[ 3.658756] (!!) init: processing action 0x1d78550 (boot)
[ 3.664256] (II) init: command 'symlink' r=0
[ 3.668588] (II) init: command 'symlink' r=0
[ 3.672953] (II) init: command 'symlink' r=0
[ 3.677250] (!!) init: processing action 0x1d787a8 (queue_propety_triggers)
[ 3.684268] (II) init: command 'queue_propety_triggers' r=0
[ 3.689865] (!!) init: processing action 0x1d77520 (property:ro.debuggable=1)
[ 3.697101] (!!) init: starting 'console'
[ ▒▒▒uid=0 gid=1007@nutshell:/ # [ 4.732175] CPU3: failed to come online
[ 4.759842] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 4.777436] ehci-mxc: Freescale On-Chip EHCI Host driver
[ 4.794683] 2184800.usbmisc supply vbus-wakeup not found, using dummy regulator
[ 4.835744] ci_hdrc ci_hdrc.1: EHCI Host Controller
[ 4.840653] ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1
[ 4.862169] ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
[ 4.868406] hub 1-0:1.0: USB hub found
[ 4.872395] hub 1-0:1.0: 1 port detected
[ 4.879079] (!!) init: waitpid returned pid 74, status = 00000000
[ 4.885222] (!!) init: process 'mount_usb', pid 74 exited

Labels (1)
0 Kudos
Reply
1 Reply

1,355 Views
igorpadykov
NXP Employee
NXP Employee

Hi Shalan

from log "Unable to handle kernel NULL pointer dereference at virtual address"

seems these errors may be related to memory, please run ddr test

i.MX6/7 DDR Stress Test Tool V2.70 

and try with some of nxp linux bsps described on

i.MX 6 / i.MX 7 Series Software and Development Tool|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply