CPU waking from sleep returns to sleep.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CPU waking from sleep returns to sleep.

2,119 Views
A_Guyula
Contributor I

I have an imx8 mini processor, trying out a wake from sleep operation.
The kernel is 5.15.32 - running Debian. 
I initiate the following to put the unit to sleep:
$ echo mem > /sys/power/state
Then I activate the wake pin. The system starts to wake up.
Looks like the cursor appears, then it falls back asleep.

My question is, if anyone has seen something like this and has a quick idea what I am doing wrong? For example, is the power state driver not clearing the state after waking?

I realize this is way out of scope, so I am not expecting much. 
Enclosed the log of why I see on the console.

Labels (2)
0 Kudos
Reply
3 Replies

2,049 Views
A_Guyula
Contributor I

We are using a Congatec SMARC board - conga-SMX8-Mini. It has 4 cores and 2Gigbytes of Ram.

I am using their variant of the 5.15.32 kernel source. The device tree is their standard device tree for this system with the addition of a modification to generate a spi device file. 

I am just hoping someone knows an "a-ha" piece of information I can examine to fix this.

0 Kudos
Reply

2,090 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @A_Guyula!

Thank you for contacting NXP Support!

 

What board are you using?

How you are configuring your device tree?

 

 

0 Kudos
Reply

2,019 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @A_Guyula!

Unfortunately the software provided for that board is custom and we can't replicate the issue.

 

Please contact to congatec support.

 

0 Kudos
Reply