CONFIG_SECURE_BOOT macro missing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CONFIG_SECURE_BOOT macro missing

1,883件の閲覧回数
supriyac
Contributor I

Hello Team,

Uboot version - 2015.07 (downloaded from git - git clone git://git.denx.de/u-boot.git)

Board - imx6q SabreSD

I was trying to enable the CONFIG_SECURE_BOOT macro according to HAB document (High_Assurance_Boot_L3.0.35_1.1.0).

Which says it is available in /include/configs/mx6q_arm2.h file.

But for the above version of uboot it is not available.

Could you please let me know, which is the alternate file that I should enable in?

-Supriya

0 件の賞賛
返信
1 返信

1,429件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Supriya

suggest to look at nxp uboot, use AN4581

uboot-imx.git - Freescale i.MX u-boot Tree

for git://git.denx.de version one can post on uboot mail list

U-Boot Info Page

L3.0.35_1.1.0 uses u-boot-2009.08.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信