CAN support on ANDROID image

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAN support on ANDROID image

2,976件の閲覧回数
sachusanal
Contributor III

Dear Sir ,

I tried to download the android soure package for sabreauto board and build it for android.

let me know i need to add CAN driver support on this android image build.

how can integrate CAN driver support on ANdroid

ラベル(1)
0 件の賞賛
返信
8 返答(返信)

2,675件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi sachu

please look at below link

How to use FlexCAN in Android OS

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,675件の閲覧回数
sachusanal
Contributor III

Hai Igor ,

I flashed prebuilt android lolipop image (which is purchased from the freescale)on sabresd board.let me know if this prebuilt image have support for CAN ?

how can i check?

0 件の賞賛
返信

2,675件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi sachu

I am afraid prebuilt image has not its support.

Best regards

igor

0 件の賞賛
返信

2,675件の閲覧回数
sachusanal
Contributor III

for Android build i hope i can refer Android user guide.

but i wanted to know for enabling the flexcan driver  what is the modification is needed

0 件の賞賛
返信

2,675件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

it is described at below link

How to use FlexCAN in Android OS

0 件の賞賛
返信

2,675件の閲覧回数
sachusanal
Contributor III

Hai Igor ,

I started the Android lolipop custom build.

i am referring android user guide for building.

from whcih step i can configure the kernel for flex can

0 件の賞賛
返信

2,675件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

it is not supported, so one should add it support using below guidelines :

How to use FlexCAN in Android OS

0 件の賞賛
返信

2,675件の閲覧回数
sachusanal
Contributor III

ok ...

Thanks for your support.

could you please help me to build android lolipop image with Flexcan driver support.

awaiting your favorable reply

Thanks

Sachu

0 件の賞賛
返信