CAN on sabresd

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN on sabresd

2,106 Views
amit251291
Contributor IV

Hello,

what are the steps to make CAN up on imx6q-sabresd board running on android 7.0?

In some previous discussions i came across https://community.nxp.com/docs/DOC-94887  this document link but this link is not opening for me. Its showing unauthorized error. I request access to this link.

Kindly guide me

0 Kudos
Reply
1 Reply

1,976 Views
igorpadykov
NXP Employee
NXP Employee

Hi Amit

according to Table 10. Supported features attached Release Notes

flexcan is not supported on i.MX6Q Sabre SD board. You can obtain some

additional details creating service request.


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply