CAN on sabresd

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAN on sabresd

2,107件の閲覧回数
amit251291
Contributor IV

Hello,

what are the steps to make CAN up on imx6q-sabresd board running on android 7.0?

In some previous discussions i came across https://community.nxp.com/docs/DOC-94887  this document link but this link is not opening for me. Its showing unauthorized error. I request access to this link.

Kindly guide me

0 件の賞賛
返信
1 返信

1,977件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Amit

according to Table 10. Supported features attached Release Notes

flexcan is not supported on i.MX6Q Sabre SD board. You can obtain some

additional details creating service request.


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信