Burning fuses

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Burning fuses

4,143件の閲覧回数
yanz
Contributor III

How can I burn fuses using NXP-MCUBootUtility tool without connect to flashloader first (there are no SW6 related GPIOs on custom board)?

Is it possible?

 

Thank you in advance

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

4,127件の閲覧回数
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @yanz,

I hope you are doing well.

Please make sure the imx board one is using is supported by NXP-MCUBootUtility.
-NXP-MCUBootUtility supports given below boards.
 i.MXRT1021, i.MXRT1051/1052, i.MXRT1061/1062, i.MXRT1064 SIP
-NXP-MCUBootUtility supports common eFuse memory operation (eFuse Programmer)

->The flash loader is responsible for initializing the microcontroller and setting up the communication channel between the microcontroller and the host computer.
->Without the flash loader, the NXP-MCUBootUtility tool will not be able to communicate with the microcontroller and access its registers to program the fuses.

Thanks & Regards,
Dhruvit Vasavada

0 件の賞賛
返信

4,104件の閲覧回数
yanz
Contributor III

The correct answer is:

It seems this is because blhost send configure-memory command to flashloader, but flashloader fail to configure flash and hung by the process. So, MCUBootUtility cannot communication with flashloader anymore.
You can set the "Boot Device" to "LPSPI NOR/EEPROM" and connect.

MCUBootUtility will not check eeprom so that it can connect successfully. After that you can scan and burn the fuse.

0 件の賞賛
返信

4,058件の閲覧回数
Dhruvit
NXP TechSupport
NXP TechSupport

Hello @yanz ,

I hope you are doing well.
Thanks for the clarification.

You can set the "Boot Device" to "LPSPI NOR/EEPROM" and connect.
MCUBootUtility will not check eeprom so that it can connect successfully. After that, you can scan and burn the fuse.


->If this answers your query, can I close this case?

Thanks & Regards,

Dhruvit Vasavada

0 件の賞賛
返信

4,056件の閲覧回数
yanz
Contributor III

Sure

0 件の賞賛
返信