Burn eFuses using MFG Tool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Burn eFuses using MFG Tool

2,066 Views
aliismail
Contributor IV

Where in the ucl2.xml document do I include the commands to burn the eFuses required to boot an image from an SD card? My best guess is after jumping to the OS image. Is this correct?

Labels (4)
0 Kudos
Reply
1 Reply

1,557 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Ali,

please take a look to the following thread.

Flashing fuses on custom imx6 board 


Regads,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------