Building fsl-image-gui on Yocto dora

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Building fsl-image-gui on Yocto dora

2,231 次查看
dominicamann
Contributor III

I have followed the excellent tutorial by Daiane Angolini to download and build yocto. When building for imx6sabresd and building fsl-image-gui, the build stops with errors about include files in EGL (there were none).Has anyone else encountered this?

标签 (3)
5 回复数

1,652 次查看
YixingKong
Senior Contributor IV

Dominic

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

Yixing

0 项奖励
回复

1,652 次查看
YixingKong
Senior Contributor IV

Dominic

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 项奖励
回复

1,652 次查看
daiane_angolini
NXP Employee
NXP Employee

Could you, please, test it again today?

This issue was fixed during this weekend.

Oh, and thanks for the compliment ^.^


1,652 次查看
LeonardoSandova
Specialist I

Which Linux flavor are you using to compile? Ubuntu 12.04 is perhaps the most tested host, at least for iMX

Leo

0 项奖励
回复

1,652 次查看
alejandrolozan1
NXP Employee
NXP Employee

Hi,

I followed the tutorial too, but I did not get any problem.

DaianeAngolini Do you have an idea of the possible problem?

Best Regards,

Alejandro

0 项奖励
回复