Building Windows 10 IOT for mcimx8m-evkb

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Building Windows 10 IOT for mcimx8m-evkb

2,236 次查看
mattasmith
Contributor I

I'm attempted to rebuild the Windows 10 IOT package is Visual Studio 2019 for the mcimx8m-evkb using the NXPEVK_iMX8M_4GB board package that is provided in the VS solution.  All of the projects appear to build without issue, but on the final step which generates the FFU (GenerateTestFFU) a lot of files appear to be missing. This is for a camera based project which will use photo compositing techniques and I would like to evaluate both Windows 10 IOT and Linux for the final solution.  Any help with the build or opinions on the right solution are welcome. imx8m-quad #windows10 iot

Log files are attached

0 项奖励
回复
1 回复

2,197 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Matthew,

There are some driver that are non-fully tested on WinIot, this is the case of camera, you can see the hardware compatibility list on:

Hardware Compatibility List - Windows IoT | Microsoft Docs 

In any case you can´t find your cameras, you will have to do the driver.

Regards

0 项奖励
回复