Build mxc_vpu_test for Android R10.3.2 -blog archive

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Build mxc_vpu_test for Android R10.3.2 -blog archive

4,657 Views
shaojun_wang
NXP Employee
NXP Employee

1. Clone linux-test from FSL git server

    git clone git://sw-git01-tx30.am.freescale.net/linux-test.git

 

2. Check out the version for r10.3.2

    git checkout 2396df8ba5af2ca4bd512dbfffeaaa8d5b5028bd

 

3. Copy vpu test code to myandroid folder and build

    mmm mxc_vpu_test

 

4. Run

    mxc-vpu-test -D "-i /mnt/sdcard/sendvpudecode.264 -f 2"

Tags (1)
0 Kudos
Reply
5 Replies

4,215 Views
satellite12
Contributor I

Hi Shaojun,

Could you help to provide the binary file?

Thanks.

0 Kudos
Reply

4,215 Views
GunjanSamaiya
Fresh Out Contributor

Initialized empty Git repository in /home/xyz/Bsp/linux-test/.git/
fatal: Unable to look up sw-git01-tx30.am.freescale.net (port 9418) (Name or service not known)

Please helpHow to Checkout ?

0 Kudos
Reply

4,215 Views
dorothyxsara
Fresh Out Contributor

Thanks a lot!

0 Kudos
Reply

4,215 Views
shaojun_wang
NXP Employee
NXP Employee

sw-git01-tx30.am.freescale.net is FSL internel link, please contact local FAE to get the source code.

0 Kudos
Reply

4,216 Views
dorothyxsara
Fresh Out Contributor

Dear sir,

fatal: Unable to look up sw-git01-tx30.am.freescale.net (port 9418)

Is this url correct?

0 Kudos
Reply