Build mfgtool firmware uboot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Build mfgtool firmware uboot

ソリューションへジャンプ
6,471件の閲覧回数
wangtsungli
Contributor IV

Hi community,

I'm working on the i.MX6 sabresd Quad platform with no PMIC.

While I try to burn image with mfgtool and I received log that show no pmic detected.

So I assumed that I need to build new uboot and kernel for mfgtool.

I had set the environment for Yocto project and try to build uboot image and kernel image with "bitbake linux-imx-mfgtool" and "bitbake u-boot-mfgtool" .

But I do not know where can I modify uboot code to avoid detecting pmic.

Question:

  1. Is there any document show how to build customize uboot and kernel for mkfgtool firmware?
  2. Is u-boot folder shared with both mfgtool firmware and image of my board?
ラベル(7)
タグ(2)
0 件の賞賛
返信
1 解決策
5,367件の閲覧回数
wangtsungli
Contributor IV

Using Yocto Project and bibake mfgtool-linux-imx for kernel firmware and bitbake u-boot-mfgtool for uboot firmware.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
5,368件の閲覧回数
wangtsungli
Contributor IV

Using Yocto Project and bibake mfgtool-linux-imx for kernel firmware and bitbake u-boot-mfgtool for uboot firmware.

0 件の賞賛
返信
5,367件の閲覧回数
jochenstehle
Contributor III

Does this provide me a single image wich include uboot, kernel and fs in a xxx.imx format that i could download it direktly via the imx_usb_loader?

0 件の賞賛
返信
5,367件の閲覧回数
wangtsungli
Contributor IV

I'm not really sure that it could do that.

But what I mentioned just can build kernel driver image and uboot image separately.

0 件の賞賛
返信
5,367件の閲覧回数
anush_deekonda
Contributor I

what are the contents of bitbake command files mfgtool-linux-imx.bb u-boot-mfgtool.bb?

0 件の賞賛
返信