cd kernel_imx
git checkout kk4.4.3_2.0.0-ga
ARCH=arm \
CROSS_COMPILE=../prebuilts/gcc/linux-x86/arm/arm-eabi-4.6/bin/arm-eabi- \
make ${JOBS} distclean
ARCH=arm \
CROSS_COMPILE=../prebuilts/gcc/linux-x86/arm/arm-eabi-4.6/bin/arm-eabi- \
make ${JOBS} imx_v7_mfg_defconfig
ARCH=arm \
CROSS_COMPILE=../prebuilts/gcc/linux-x86/arm/arm-eabi-4.6/bin/arm-eabi- \
make uImage LOADADDR=0x10008000
CC kernel/power/earlysuspend.o
kernel/power/earlysuspend.c: In function 'early_suspend':
kernel/power/earlysuspend.c:109:3: error: implicit declaration of function 'android_wake_unlock' [-Werror=implicit-function-declaration]
kernel/power/earlysuspend.c: In function 'request_suspend_state':
kernel/power/earlysuspend.c:173:3: error: implicit declaration of function 'android_wake_lock' [-Werror=implicit-function-declaration]
cc1: some warnings being treated as errors
make[2]: *** [kernel/power/earlysuspend.o] Error 1
make[1]: *** [kernel/power] Error 2
make: *** [kernel] Error 2
Hi,
Mfg confg did not set android config, so when use android function will build fail.
It is because Mfg kernel is use linux kernel, you can switch to linux branch like imx_3.10.53_1.1.0_ga. And $make imx_v7_mfg_defconfig will build successfully.
Or you can replace the ~myandroid/kernel_imx/.config file with attach file, and will build successfully.
Best Regards,
Alejandro
Hi
huang kc
Use Yocto build to generate kernel for mfgtool.
I have the same mistake, and i had to use yocto build.
But i can not booting after i replace the zImage in mfgtools.
It will be stop when the system check emmc.
mmc3: BKOPS_EN bit is not set
mmc3: new high speed DDR MMC card at address 0001
mmcblk3: mmc3:0001 S10008 7.28 GiB
mmcblk3boot0: mmc3:0001 S10008 partition 1 4.00 MiB
mmcblk3boot1: mmc3:0001 S10008 partition 2 4.00 MiB
mmcblk3rpmb: mmc3:0001 S10008 partition 3 4.00 MiB
mmcblk3: p1 p2 p3 < p5 p6 p7 > p4
mmcblk3: p4 size 13090816 extends beyond EOD, truncated
mmcblk3boot1: unknown partition table
mmcblk3boot0: unknown partition table
Do you know what is happened?
Hello Saurabh,
Thank you for your help. However, it doesn't make sense for customer to maintain two version of kernel if only develop Android project. Truly wish Freescale can solve this issue soon.