Build Failure for I.MX53 QSB source.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Build Failure for I.MX53 QSB source.

2,709件の閲覧回数
anandasagar
Contributor I

Hi,

        I have followed the Release notes from Adeneo to download the android source for i.mx53 qsb (Android GingerBread V4.3), but facing problem while building the android source. I have applied the android and qsb patches following the steps in the release note. But when i am trying to build the android source with  "./build_android.sh --board=imx53_qsb --build-choice=android --lunch-type=eng". i am observing segmentation fault.

Please see the logs below.

################################################

Building for imx53_qsb:

  BUILD_UBOOT=0

  BUILD_KERNEL=0

  BUILD_ANDROID=1

Android Lunch type: eng

Using:

  CPUS_KERNEL=1

  CPUS_ANDROID=1

################################################

./build_android.sh: line 262:  5640 Segmentation fault      make PRODUCT-${ANDROID_CFG}-${LUNCH_TYPE} -j${CPUS_ANDROID}

Image Name:   Android Root Filesystem

Created:      Thu Apr 18 09:02:06 2013

Image Type:   ARM Linux RAMDisk Image (uncompressed)

Data Size:    182409 Bytes = 178.13 kB = 0.17 MB

Load Address: 70308000

Entry Point:  70308000

cp: cannot stat `system.img': No such file or directory


Please let me know what i might be possibly missing! and help me resolve this problem. Thanks

0 件の賞賛
返信
3 返答(返信)

1,928件の閲覧回数
Yuri
NXP Employee
NXP Employee

Android build-system requires a 64-bit machine, for 32-bit host special patch may be needed.

0 件の賞賛
返信

1,928件の閲覧回数
anandasagar
Contributor I

Hi Muhin thanks for the reply, i am building it on 64bit machine itself, but still facing the problem, any possible reason for it ?

0 件の賞賛
返信

1,928件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

Deactivated user can you help on this case?

0 件の賞賛
返信