Bug in fec.c linux 2.6.31 sdk L2.6.31_09.12.01_SDK_SOURCE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Bug in fec.c linux 2.6.31 sdk L2.6.31_09.12.01_SDK_SOURCE

2,023 次查看
Matt_
Contributor II

file linux-2.6.31/drivers/net/fec.c

The fec_set_mac_address function has a line:

writel((dev->dev_addr[5] << 16) | (dev->dev_addr[4] << 24),
        fep + FEC_ADDR_HIGH);

which should read:

writel((dev->dev_addr[5] << 16) | (dev->dev_addr[4] << 24),
        fep->hwp + FEC_ADDR_HIGH);

Writing to fep + FEC_ADDR_HIGH causes strange crashes and it took some time to find it was this function clobbering some-one else's data.

 

I hope this helps some-one.

 

 Matt.

标记 (1)
0 项奖励
回复
6 回复数

1,829 次查看
fabio_estevam
NXP Employee
NXP Employee

Darron,

It is a good idea to use the mainline kernel if you can.

Currently not all the support available on FSL 2.6.35 kernel is available in mainline, but the kernel mainline support for MX28 is growing. As of 3.2-rc1 kernel there are 3 MX28-base boards available there:

MX28EVK, TX28 and M28EVK

 

Regards,

 

Fabio Estevam


Darron Black said:

Fabio,

Is this true in the general case?  Should I be on the latest 3.x kernel with i.MX28x?  Have all the patches from 2.6.35.3+ from the board support packages made it into mainline now?


Fabio Estevam said:

If you are interested in a more recent kernel for mx35 you can use the latest 3.1 kernel.

It does provide support for mx35pdk as well as other mx35-based boards.

0 项奖励
回复

1,829 次查看
Matt_
Contributor II

Thanks Fabio,

The product's about to hit the street and so I don't wish to jump kernels at this time.

Fabio Estevam said:

If you are interested in a more recent kernel for mx35 you can use the latest 3.1 kernel.

It does provide support for mx35pdk as well as other mx35-based boards.

0 项奖励
回复

1,829 次查看
darron
Contributor I

Fabio,

Is this true in the general case?  Should I be on the latest 3.x kernel with i.MX28x?  Have all the patches from 2.6.35.3+ from the board support packages made it into mainline now?


Fabio Estevam said:

If you are interested in a more recent kernel for mx35 you can use the latest 3.1 kernel.

It does provide support for mx35pdk as well as other mx35-based boards.

0 项奖励
回复

1,829 次查看
fabio_estevam
NXP Employee
NXP Employee

If you are interested in a more recent kernel for mx35 you can use the latest 3.1 kernel.

It does provide support for mx35pdk as well as other mx35-based boards.

0 项奖励
回复

1,829 次查看
Matt_
Contributor II
Thanks.  Hopefully Freescale will update the download area of the i.MX35 parts to use the later kernel.

Darron Black said:
I'm using the 2.6.35 kernel, and it appears it's already been fixed in that version.
0 项奖励
回复

1,829 次查看
darron
Contributor I
I'm using the 2.6.35 kernel, and it appears it's already been fixed in that version.
0 项奖励
回复