Broadcom wifi power management issue .

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Broadcom wifi power management issue .

3,101 Views
veeranjaneyulug
Contributor III

Hi every one,

we used yocto setup and kernel 3.14.28 .Than i gave bitbake wl commnad but its showing nothing providers.i want wl tool for imx6 target board.can you any body guide me.

And how to test wifi standby mode and sleep mode on imx6 target board.

I will use commands :

wl PM0

wl PM1

I will use but I dont have wl tool for imx6 target board.first how to get wl binay for imx6 target board.

Thanks & Regards

veeranjaneyulu

0 Kudos
Reply
2 Replies

2,722 Views
igorpadykov
NXP Employee
NXP Employee

Hi veeranjaneyulu

these modules are supported starting from 3.14.38 kernel,

3.14.28 supports AR6003 as shown in attached Release Notes.

Suggest to contact broadcom support for driver.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,722 Views
veeranjaneyulug
Contributor III

Thanks Igor ,

I will check .

0 Kudos
Reply