Brightness control from UVC endpoint

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Brightness control from UVC endpoint

2,002 Views
Bariel76
Contributor II

Hi All,

It is my first time with a UVC endpoint. I read a lot on the protocol in the last days. But I still have problem using the options of the processing unit descriptors.

 

Here is a little context:

I merged the "evkmimxrt1060_dev_video_virtual_camera_bm" demo project with the "evkmimxrt1060_csi_raw8" project. 

I am able to get a video feed in RGB565 format from the MT9M114 camera. I use opencv2 in python to get the feed.

I am using the UVC class version 1.1.

 

Here is the problem:

I set the processing descriptors to unable the brightness control

 

 

    /* Processing Unit Descriptor start*/
    USB_VIDEO_VIRTUAL_CAMERA_VC_PROCESSING_UNIT_LENGTH, /* Size of this descriptor, 10+n */
    USB_DESCRIPTOR_TYPE_VIDEO_CS_INTERFACE,             /* CS_INTERFACE, descriptor type */
    USB_DESCRIPTOR_SUBTYPE_VIDEO_VC_PROCESSING_UNIT,    /* VC_PROCESSING_UNIT, descriptor subtype */
    USB_VIDEO_VIRTUAL_CAMERA_VC_PROCESSING_UNIT_ID,     /* A non-zero constant that uniquely identifies the
                                                           Terminal within the video function. This value is
                                                           used in all requests to address this Terminal. */
    USB_VIDEO_VIRTUAL_CAMERA_VC_INPUT_TERMINAL_ID,      /* ID of the Unit or Terminal to which this Terminal is
                                                           connected */
    0x00U, 0x00U, /* This field indicates the maximum digital magnification, multiplied by 100U */
    0x02U,        /* Size of the bmControls field, in bytes: n */
    0x00U, 0x01U, /* Brigthness control */

    0x00U, /* A bitmap of all analog video standards supported by the Processing Unit */

 

 

 

 However, when I send the following, there is not breakpoint I can place anywhere that will get triggered. 

cap = cv2.VideoCapture(1)
exposure = cap.set(cv2.CAP_PROP_BRIGHTNESS, 0.1)

 Any ideas on how to make this work?

0 Kudos
Reply
2 Replies

1,987 Views
Bariel76
Contributor II

Ok, I have found the function in usb_device_video.c. 

 

 

USB_DeviceVideoVcProcessingUnitRequest

 

 

However, the openCV command below does not trigger the function. Does openCV need UVC version 1.5 in order to work? What am I missing?

 

exposure = cap.set(cv2.CAP_PROP_BRIGHTNESS, 1)

 

 

0 Kudos
Reply

1,958 Views
nxf77486
NXP TechSupport
NXP TechSupport

Hello,

 

Thank you for contacting NXP support.

We have the following application note that explain how to implement and use an UVC device on the RT. I think this could be helpful as a guide for your project.

Please let me know if there is anything else where I can help you.

0 Kudos
Reply