Boundary Scan on IMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Boundary Scan on IMX6

1,448 Views
Wei
Contributor I

According to ERR009218 of IMX6DQCE, Boundary scan test will fail to drive outputs on the signals listed above. These signals can be tested as input-only.

How to make these pins outoupt correct value to enable full JTAG access on EIM?

0 Kudos
Reply
1 Reply

1,372 Views
Yuri
NXP Employee
NXP Employee

Hello,

  I've sent You some considerations directly.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply