Boundary Scan on IMX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Boundary Scan on IMX6

1,438件の閲覧回数
Wei
Contributor I

According to ERR009218 of IMX6DQCE, Boundary scan test will fail to drive outputs on the signals listed above. These signals can be tested as input-only.

How to make these pins outoupt correct value to enable full JTAG access on EIM?

0 件の賞賛
返信
1 返信

1,362件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  I've sent You some considerations directly.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信