Booting linux from NAND Flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Booting linux from NAND Flash

3,237 Views
cnguyenterasci
Contributor I

When I boot my device from NAND flash, everything goes ok but it just stops booting at "Waiting for root device /dev/mmcblk0p3..."

Labels (2)
0 Kudos
Reply
5 Replies

2,904 Views
cnguyenterasci
Contributor I

I ran the MFG Tool and loaded linux on the NAND flash.  I h ave the jumpers set to be booting from NAND flash as well. 

0 Kudos
Reply

2,903 Views
jimmychan
NXP TechSupport
NXP TechSupport

When the board booting up, there is a "Kernel Command line". Please check the root filesystem location. it should be something like "root=/dev/xxxxxxxx". For NAND, should be like this root=/dev/mtdblock1.

2,903 Views
jimmychan
NXP TechSupport
NXP TechSupport

Is your filesystem store in the SD Card? according to your message, it is looking for the rootfs from the SD Card (mmcblk0) partition 3. Please double check the bootargs in uboot used is correct or not.

0 Kudos
Reply

2,903 Views
sinanakman
Senior Contributor III

Calvin, which device, which board is this ?

0 Kudos
Reply

2,903 Views
cnguyenterasci
Contributor I

i.Mx233.  I have an EVK board as well as a board I designed and I get the same thing on both boards.

0 Kudos
Reply