Booting from SPI NAND flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Booting from SPI NAND flash

2,750 Views
syuriks
Contributor I

Hello,

 Is it possible to use SPI NAND flash as a boot device on i.MX8 processors?

Thanks in advance,

Yuri

0 Kudos
Reply
3 Replies

2,454 Views
syuriks
Contributor I

Just to clarify: in both chipsets i.MX8QXP and i.MX8M is there boot ROM firmware limitation or is there some HW limitation?

Thanks you in advance,

Yuri

0 Kudos
Reply

2,454 Views
igorpadykov
NXP Employee
NXP Employee

it is ROM limitation.

Best regards
igor

0 Kudos
Reply

2,454 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuri

seems not, i.MX8QXP supports FlexSPI NOR flash boot, i.MX8M boot ROM

only supports :
• NAND flash
• SD/MMC

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply