Booting M7 and A53 core with separate OS in iMX8 Nano

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Booting M7 and A53 core with separate OS in iMX8 Nano

2,503件の閲覧回数
anurag16doshi
Contributor III

I want to boot the iMX8 Nano EVK board with 2 separate OS on the A53 core and the M7 core. I want them to boot independently from each other. I have read through the available documentation for the board and the cores as well. I still haven't found a solution for the same. I want to run the m7 with FreeRTOS on it and the A53 with Android on it.

Am I missing some document that helps me do this? Or is there a way to boot the OS independently of each other from SD/eMMC or any other way?

TIA,

Anurag

0 件の賞賛
返信
2 返答(返信)

2,435件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Anurag,

Sorry not in android, you can refer to "Running the Arm Cortex-M4 image" of Linux User's Guide for running the M4 image.

Regards

0 件の賞賛
返信

2,417件の閲覧回数
kippowens
Contributor IV

Is there an OS combo where booting to the M7 as the main is possible?

0 件の賞賛
返信