Booting Linux Kernel For imx6 UL EValution kit(ImxULevk)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Booting Linux Kernel For imx6 UL EValution kit(ImxULevk)

1,275件の閲覧回数
nagaprasadvasam
Contributor III

Hi everyone,

I need some Information regarding MACHINE selection in Yocto build procedure for my board which machine i need to select for imxULevk . can any one help me?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,158件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Helo Nagaprasad Vasamsetti,

You can see the available MACHINES on any particular BSP released listed on the Build Configurations section of the Freescale Yocto Project User’s Guide included as part of the BSP documentation.

If you are using the Community BSP this information is available on the Supported Board List available on the Community BSP documentation.

The MACHINE that corresponds to the i.MX6UL EVK in both BSPs is: “imx6ulevk”

I hope this information helps!

Regards,

0 件の賞賛
返信

1,158件の閲覧回数
nagaprasadvasam
Contributor III

hi,

Thanks for your information,can you please provide a link for Building yocto For imx6ULevk.

Thanks&Regards,

Nagaprasad.

0 件の賞賛
返信