Boot-up support using SD interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Boot-up support using SD interface

1,459件の閲覧回数
mrudangshelat
Contributor IV

Hi, I am using iMX6D in my new design and I would like to to boot using SD and eMMC. There are total 4 SD interface available on iMX6D. I just wanted to confirm that can I use all 4 SD interface (SD1, SD2, SD3 and SD4) to Boot-up iMX6D using SD and eMMC? I have also read that "SDR50 and SDR104 boot are not supported on the USDHC1 and USCHD2 ports because there are no reset signals for those ports is connected in the IOMUX." from iMX6 Reference manual. Please provide your valuable view. Thanks, Mrudang

ラベル(2)
0 件の賞賛
返信
1 返信

1,365件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Mrudang

right, one can use all 4 SD interfaces.

For booting one can use High Speed mode, some

overview can be found on p.184 http://cache.freescale.com/files/32bit/doc/errata/IMX6DQCE.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信