Boot from Serial flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Boot from Serial flash

1,331 Views
asou_junichi
Contributor I

Hi,

If i.MX6 is accidentally restarted during accessing to the serial flash at upper 128Mb segment with 4-byte addressing mode.

Then i.MX6 tries to reboot from the serial flash with 3-byte addressing mode but the serial flash still stays in 4-byte addressing mode. 

In this case, the serial flash can not be read correctly because there are mismatch of addressing mode between i.MX6 and serial flash.

To avoid this kind of issue, dose the serial flash with hardware reset pin have to be introduced, and resetting the serial flash when i.MX6 is rebooting?

Or are there any other idea?

BR,

JA

Labels (1)
0 Kudos
Reply
1 Reply

1,279 Views
igorpadykov
NXP Employee
NXP Employee

Hi 麻生 淳一 

>dose the serial flash with hardware reset pin have to be introduced, and resetting

>the serial flash when i.MX6 is rebooting?

yes this is correct idea.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply