Boot from SATA ISSUES

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Boot from SATA ISSUES

1,086 Views
Chicago1984
Contributor II

I was able to blow the fuse and see that the boot device is now SATA, but now I’m getting a “Card

did not respond to voltage select!” and “MMC init failed” error.  I wonder if there is something in

the code that is still wanting to grab code from the SD card.

Is there an easy way to blow the fuse in the Manufacturing Tool?  I tried to set it up, but being new

to it I was getting no ware slowly.

Image attached.

Labels (1)
0 Kudos
Reply
2 Replies

833 Views
tonyzheng
NXP Employee
NXP Employee

Hello,

It seems that you board is not the official reference board powered by Freescale.

Can you tell me where your kernel and rootfs, in SATA or SD card?

As with SadreSD board, booting from the SATA is supported through changing u-boot configs.

0 Kudos
Reply

833 Views
tonyzheng
NXP Employee
NXP Employee

If your kernel and rootfs reside in the SATA SSD, you don't need to detect SD Card.

For more information, you can refer to:

https://community.freescale.com/message/318957#318957

0 Kudos
Reply