I am using imx6 solo processor and trying to boot from micron MLC nand. I tried to write u-boot.imx image from kobs-ng.
I am not sure weather u-boot image is properly written in nand or not.
Can anyone help in finding the way to verify weather boot image written in nand is proper or not.
Also I need help in getting u-boot commands to initiate boot from nand.
Command : kobs-ng init -v -x u-boot.imx
LOG Message :
MTD CONFIG:
chip_0_device_path = "/dev/mtd0"
chip_1_device_path = "(null)"
search_exponent = 2
data_setup_time = 80
data_hold_time = 60
address_setup_time = 25
data_sample_time = 6
row_address_size = 3
column_address_size = 2
read_command_code1 = 0
read_command_code2 = 48
boot_stream_major_version = 1
boot_stream_minor_version = 0
boot_stream_sub_version = 0
ncb_version = 3
boot_stream_1_address = 0
boot_stream_2_address = 0
u-boot.imx_solo: verifying using key '00000000000000000000000000000000'
u-boot.imx_solo: is a valid bootstream for key '00000000000000000000000000000000'
mtd: opening: "/dev/mtd0"
mtd: opened '/dev/mtd0' - '(null)'
mtd: max_boot_stream_size_in_bytes = 4194304
mtd: boot_stream_size_in_bytes = 425856
mtd: boot_stream_size_in_pages = 104
mtd: #1 0x00200000 - 0x00600000 (0x00267f80)
mtd: #2 0x00600000 - 0x00a00000 (0x00667f80)
FCB
m_u32Checksum = 0
m_u32FingerPrint = 541213510
m_u32Version = 16777216
m_NANDTiming.m_u8DataSetup = 80
m_NANDTiming.m_u8DataHold = 60
m_NANDTiming.m_u8AddressSetup = 25
m_NANDTiming.m_u8DSAMPLE_TIME = 6
m_u32PageDataSize = 4096
m_u32TotalPageSize = 4320
m_u32SectorsPerBlock = 256
m_u32NumberOfNANDs = 0
m_u32TotalInternalDie = 0
m_u32CellType = 0
m_u32EccBlockNEccType = 8
m_u32EccBlock0Size = 512
m_u32EccBlockNSize = 512
m_u32EccBlock0EccType = 8
m_u32MetadataBytes = 10
m_u32NumEccBlocksPerPage = 7
m_u32EccBlockNEccLevelSDK = 0
m_u32EccBlock0SizeSDK = 0
m_u32EccBlockNSizeSDK = 0
m_u32EccBlock0EccLevelSDK = 0
m_u32NumEccBlocksPerPageSDK = 0
m_u32MetadataBytesSDK = 0
m_u32EraseThreshold = 0
m_u32Firmware1_startingPage = 512
m_u32Firmware2_startingPage = 1536
m_u32PagesInFirmware1 = 104
m_u32PagesInFirmware2 = 104
m_u32DBBTSearchAreaStartAddress = 256
m_u32BadBlockMarkerByte = 3904
m_u32BadBlockMarkerStartBit = 0
m_u32BBMarkerPhysicalOffset = 4096
m_u32BCHType = 0
m_NANDTMTiming.m_u32TMTiming2_ReadLatency = 0
m_NANDTMTiming.m_u32TMTiming2_PreambleDelay = 0
m_NANDTMTiming.m_u32TMTiming2_CEDelay = 0
m_NANDTMTiming.m_u32TMTiming2_PostambleDelay = 0
m_NANDTMTiming.m_u32TMTiming2_CmdAddPause = 0
m_NANDTMTiming.m_u32TMTiming2_DataPause = 0
m_NANDTMTiming.m_u32TMSpeed = 0
m_NANDTMTiming.m_u32TMTiming1_BusyTimeout = 0
m_u32DISBBM = 0
DBBT
m_u32Checksum = 0
m_u32FingerPrint = 1413628484
m_u32Version = 16777216
m_u32DBBTNumOfPages = 0
Firmware: image #0 @ 0x200000 size 0x68000 - available 0x400000
Firmware: image #1 @ 0x600000 size 0x68000 - available 0x400000
-------------- Start to write the [ FCB ] -----
mtd: erasing @0:0x0-0x100000
mtd: Writing FCB0 [ @0:0x0 ] (10e0) *
mtd: Writing FCB1 [ @0:0x40000 ] (10e0) *
mtd: Writing FCB2 [ @0:0x80000 ] (10e0) *
mtd: Writing FCB3 [ @0:0xc0000 ] (10e0) *
mtd_commit_bcb(FCB): status 0
-------------- Start to write the [ DBBT ] -----
mtd: erasing @0:0x100000-0x200000
mtd: Writing DBBT0 [ @0:0x100000 ] (1000) *
mtd: Writing DBBT1 [ @0:0x140000 ] (1000) *
mtd: Writing DBBT2 [ @0:0x180000 ] (1000) *
mtd: Writing DBBT3 [ @0:0x1c0000 ] (1000) *
mtd_commit_bcb(DBBT): status 0
---------- Start to write the [ u-boot.imx_solo ]----
mtd: Writting u-boot.imx_solo: #0 @0: 0x00200000 - 0x00268000
mtd: erasing @0:0x200000-0x300000
mtd: The last page is not full : 3968
mtd: We write one page for save guard. *
mtd: Writting u-boot.imx_solo: #1 @0: 0x00600000 - 0x00668000
mtd: erasing @0:0x600000-0x700000
mtd: The last page is not full : 3968
mtd: We write one page for save guard. *
COMMAND : kobs-ng dump -v u-boot.imx_solo
MTD CONFIG:
chip_0_device_path = "/dev/mtd0"
chip_1_device_path = "(null)"
search_exponent = 2
data_setup_time = 80
data_hold_time = 60
address_setup_time = 25
data_sample_time = 6
row_address_size = 3
column_address_size = 2
read_command_code1 = 0
read_command_code2 = 48
boot_stream_major_version = 1
boot_stream_minor_version = 0
boot_stream_sub_version = 0
ncb_version = 3
boot_stream_1_address = 0
boot_stream_2_address = 0
mtd: opening: "/dev/mtd0"
mtd: opened '/dev/mtd0' - '(null)'
mtd: partition #0
type = 8
flags = 1024
size = 10485760
erasesize = 1048576
writesize = 4096
oobsize = 224
blocks = 10
Segmentation fault
U-boot command used :
mw.l 0x20d8040 0x1683
mw.l 0x20d8044 0x10000000
reset
But it is not getting booted.
Reference Used : Freescale Yocto i.MX6 U-Boot NAND Boot
Thanks in advance
Hi sanjay
had you added in image support for this new NAND to
drivers/mtd/nand/nand_ids.c
drivers/mtd/nand/nand_device_info.c ?
kobs-ng uses info in these files while writing to NAND.
Also recommended way to use MFG Tool (Sabre AI profile has
script for NAND writing)
IMX_6_MFG_L3.10.17_1.0.0_TOOL
: i.MX 6Family Manufacturing Toolkit for L3.10.17.
Actually for testing you can try with older ltib release
IMX_6DL_6S_MFG_TOOL
: Tool and documentation for downloading OS images to the i.MX 6DualLite and i.MX6Solo.
Best regards
igor
Hi Igor
Thanks for your reply.
I am using micron NAND flash and it is getting detected by kernel. Nand device is working fine so, I don't think there is any need of adding support in nand_ids.c.
I am having a doubt :
How can we set the bootable device as nand?
I am using command in u-boot cmd prompt:
mw.l 0x20d8040 0x1683
mw.l 0x20d8044 0x10000000
reset
Is it correct for imx6_solo.
Regards
Sanjay
Hi Sanjay
how is implemented WDOG reset on your board ?
Does it also toggle PMIC PWRON as in p.21 SPF-27392.
This is recommended reset circuit and with it anything, which you wrote
in Uboot to GPR9,10 will be reset to 0. Boot will be performed using boot pins
or from fuses as described in Chapter 8 System Boot IMX6SDLRM
Best regards
igor
Hi Igor,
We tried with SPI NOR Flash and device is booting.
I am not sure about WDOG reset on board. But to boot from SPI NOR, we need to configure GPR 9 and 10.
Also I am not sure about PMIC POWERON toggle circuitry.
Regards
Sanjay
Hi Sanjay
could you point to documents which
described usage GPR 9 and 10 while booting
from SPI NOR ?
Best regards
igor
Hi Igor
"After reset, if GPR10[28] is 1, ROM will copy GPR9[25:0] to SBMR1, which will determine the boot device."
I got this statement about software reset from link :
http://lists.denx.de/pipermail/u-boot/2012-May/125283.html
command I am using for booting from SPI NOR :
mw.l 0x20d8040 0x18000030
mw.l 0x20d8044 0x10000000
reset
Regards
Sanjay
Hi Sanjay
you can boot from NAND then read SBMR1,
after that try use this value with uboot mw..reset commands
Best regards
igor
Hi Igor,
I am not able to beet from NAND. How can I proceed further?
I tried with MFG tool also.
MFG is not able to write u-boot image into the nand.
I cross checked the image written in NAND using kobs-ng and it seems to be placed in correct address with 1K of padding.
FCB and DBBT is also placed at desired address.
As 1st 2MB is reserved for FCB and and DBBT so u-boot starts from 2MB+1k address.
NAND Description :
Manufacturer ID: 0x2c, Chip ID: 0x68
Micron MT29F32G08CBACAWP
4096MiB, MLC, page size: 4096, OOB size: 224
Regards
Sanjay
Hi Sanjay
you can check SBMR1 with jtag.
Best regards
igor