Boot configure voltage

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Boot configure voltage

1,680件の閲覧回数
van-tuongpham
Contributor I

Hi experts,

We are design board based on IMX8M mini ref board. Because of voltage level, we change voltage of SAI1/2, GPIOs, I2Cs, to 3V3. As SPF-35104_B1 and SPF-31407_C2, BOOT_MODE0/1 using VDD_1V8 pullup. Can I change to VDD_3V3? Is that change affected by sequence of Power?

Thanks

ラベル(2)
0 件の賞賛
返信
1 返信

1,558件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Van-Tuong

allowable voltages are described in Table 9. Operating ranges

i.MX 8M Mini Applications Processor Datasheet for Consumer Products

for pad power supply one can look at Table 64. i.MX 8M Mini 14 x 14 mm functional

contact assignments, column "Power group".

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信