Boot SPL from boot partition for a custom board using imx6ull

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Boot SPL from boot partition for a custom board using imx6ull

ソリューションへジャンプ
2,830件の閲覧回数
brinda-bhatt
Contributor II

Hello all, 

How to boot SPL from boot partition of emmc for my custom board using imx6ull?

When i flash my SPL to user partition using the below command, it boots as expected.

dd if=SPL of=/dev/mmcblk0 bs=1k seek=1 conv=sync

But doing the same with boot partition doesn't work. Can someone help?

0 件の賞賛
返信
1 解決策
2,769件の閲覧回数
brinda-bhatt
Contributor II

The issue is resolved.

There was no problem with imx side. Changing the configuration register of emmc to enable boot partition resolved the issue. 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,770件の閲覧回数
brinda-bhatt
Contributor II

The issue is resolved.

There was no problem with imx side. Changing the configuration register of emmc to enable boot partition resolved the issue. 

0 件の賞賛
返信
2,823件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Brinda

 

one can try to select partition with "mmcdev" as described in  i.MX Linux User’s Guide​

sect.4.7.6 Running Linux OS from MMC/SD

Also may be useful:

https://boundarydevices.com/programming-emmc-on-i-mx6/

 

Best regards
igor

0 件の賞賛
返信
2,814件の閲覧回数
brinda-bhatt
Contributor II

Thanks for your prompt reply.

This guides talk about booting linux OS from emmc. I achieved that part already.

But i am stuck at booting SPL from emmc. I would like to use boot partition of emmc to store SPL & boot. But it works only with user partition.

0 件の賞賛
返信