First, i have compiled and installed the LTIB contained in the package L2.6.35_11.03.00_ER_source.tar.gz under Ubuntu 10.04 on a real machine (no VM) according to the steps described in the documents "i.MX53 START Linux" and ltib_build_host_setup.pdf.
Then i configured LTIB for the i.MX53 QSB as target. The compilation finished without errors
and the /rootfs folder was created successfully. I have flashed and setup u-boot to the micro-sd.
When i start the board first the kernel is loaded successfully over ethernet from the host. The kernel
then mounts the /rootfs directory via NFS. But then after loading many modules
the startup aborts with the following error message in the serial terminal:
...
gtk: creating gdk-pixbuf.loaders
pango: creating module list
starting pid 2218, tty '': '/sbin/getty -L ttymxc0 115200 vt100'
(EE) XKB: Couldn't open rules file /usr/share/X11/xkb/rules/base
(EE) XKB: No components provided for device Virtual core keyboard
Backtrace (0 deep):
Fatal server error:
Segmentation fault caught
Can't deallocate console 2 Device or resource busy
arm-none-linux-gnueabi-gcc (4.4.4_09.06.2010) 4.4.4
root filesystem built on Wed, 11 May 2011 17:47:44 +0200
Freescale Semiconductor, Inc.
freescale login: matchbox-panel: failed to open displaymatchbox-desktop: unable to open display !
matchbox: can't open display! check your DISPLAY variable.
ts_open: No such file or directory
I have checked the folder /usr/share/X11 which contains only a text file. I have compared
the own generated rootfs with the rootfs contained in the demo image L2.6.35_11.03.00_ER_images_MX5X.tar.gz and it seams that many of files for X11 do not exist.
Is there a need to manually install packages with LTIB to the own build /rootfs ? I have checked
that all X11 packages are selected in LTIB before build the rootfs.
I have also tried the 11.01 packages but the behavior is the same.
What is wrong?
I have attached the complete output in the serial terminal and the u-boot configuration.
Hello Claude,
i still have the error :(
root@freescale ~$ export DISPLAY=:0.0
root@freescale ~$ Xfbdev -nolisten tcp -mouse mouse,,device=/dev/input/mice -key
bd keyboard,,/dev/input/event4 &
root@freescale ~$ (EE) XKB: Couldn't open rules file /usr/share/X11/xkb/rules/base
(EE) XKB: No components provided for device Virtual core keyboard
Kbd option key (/dev/input/event4) of value ((null)) not assigned!
(EE) XKB: Couldn't open rules file /usr/share/X11/xkb/rules/base
(EE) XKB: No components provided for device (unnamed keyboard)
Hello guys,
After build QT i've tried to run a sample but unsuccessful.
I got this error:
root@freescale ~$ export DISPLAY=:0.0
root@freescale ~$ Xfbdev -mouse mouse,,device=/dev/input/mice -keybd keyboard,,/dev/input/event2 &
root@freescale ~$ _XSERVTransSocketOpenCOTSServer: Unable to open socket for inet6
_XSERVTransOpen: transport open failed for inet6/freescale:0
_XSERVTransMakeAllCOTSServerListeners: failed to open listener for inet6
(EE) XKB: Couldn't open rules file /usr/share/X11/xkb/rules/base
(EE) XKB: No components provided for device Virtual core keyboard
Kbd option key (/dev/input/event2) of value ((null)) not assigned!
(EE) XKB: Couldn't open rules file /usr/share/X11/xkb/rules/base
(EE) XKB: No components provided for device (unnamed keyboard)
The error you saw is related to touch screen.
You can add the following changes in your rootfs /usr/bin/startx:
if [ -L /dev/input/ts0 ]; then
Xfbdev -mouse tslib,2,device=/dev/input/ts0 -mouse mouse,2,device=/dev/input/mice&
else
Xfbdev -mouse mouse,2,device=/dev/input/mice&
fi
If no touch screen is detected, don't initialize touch screen for Xfbdev.