BogoMIPS : 3.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BogoMIPS : 3.0

2,346 Views
jialu
Contributor II

1.jpg

Why BogoMIPS is 3.00? What does 3.00 means?

Labels (2)
0 Kudos
Reply
3 Replies

2,229 Views
igorpadykov
NXP Employee
NXP Employee

Hi XU

please look on

BogoMips - Wikipedia 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,229 Views
jialu
Contributor II

Just 3.00?

In my PC, it's value is 5184.00.

Is there some thing wrong here?

3Q

0 Kudos
Reply

2,229 Views
igorpadykov
NXP Employee
NXP Employee

you can try kernel 3.0.35 which had correct value.

change happens since:  commit 1119c84aa3053bd415ba731ada1ecef24c8f82a2
Author: Sebastian Andrzej Siewior <[email protected]>
Date: Wed Jan 22 12:35:44 2014 +0100

ARM: imx: enable delaytimer on the imx timer

The imx can support timer-based delays, so implement this.
Skips past jiffy calibration.

0 Kudos
Reply