Bluetooth paring not working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bluetooth paring not working

2,319件の閲覧回数
jemish_1990
Contributor V

Hi All,

We are using WL18XX TiWilink module in our project with IMX6Q based customized board.

To make WL18XX module working we followed steps suggested on "Step-by-step: How to setup TI Wilink (WL18xx) with iMX6 Linux 3.10.53 " . By following steps suggested on this link we are able to make Wifi and Bluetooth module working.  We are able to make "hci0" interface up and scanning working.

The problem is after scanning nearby devices we are not able to pair/connect that device with bluetooth of our board.

Is there any packages/utilities available to make it working?

Our end use case is to make bluetooth audio working but before that we need to pair it first.

As this project is crucial stage to finalize board layout only verification of Bluetooth audio is remaining thing.

Any suggestion for this issue will be appreciated. Please let me know if any information required from my side.

Thanks,

Jemish

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,961件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jemish

one can try ask for updated firmware for used module from ti and

post issue on wl18x wiki: WL18xx - Texas Instruments Wiki

Best regards

igor

0 件の賞賛
返信

1,961件の閲覧回数
jemish_1990
Contributor V

Hi igor,

I am sure that it is not firmware issue. Because I am able to make interface up and and scan near by devices.

The issue is with TI's recommended Bluetooth Stack which has few hard codings according to their kernel.

Because of this it always shows Device in Power down state. I have already posted query on ti e2e community.

I am discussing this issue with them.

https://e2e.ti.com/support/wireless_connectivity/wilink_wifi_bluetooth/f/307/p/497409/1800727#180072...

Meanwhile can you provide steps / documentation for open source bluetooth stack which I can try to make pairing working.

Thanks,

Jemish

0 件の賞賛
返信

1,961件の閲覧回数
jemish_1990
Contributor V

Hi,

We have make it working using TI's help so we can close this thread now.

Thanks,

Jemish

0 件の賞賛
返信