Bluetooth and WLAN do not work together ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bluetooth and WLAN do not work together ?

1,539件の閲覧回数
weikeng-jimmy
Contributor III

Hi Sir,

Android kk4.4 Release_Notes have a known issue is Bluetooth and WLAN do not work together. My customers ask the issue is caused by Freescale BSP ?

Or by Silex AR6233X SDIO module ? Have any update for solved Schedule ? Thanks!

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,337件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Hello Jimmy,

WLAN and BT radios utilize hardware coexistence signaling between the devices. We only have old version for this tool which is based on bluez and the old wifi driver. You need to contact the vendor to supply new version tool to support it.


Have a great day,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,337件の閲覧回数
mutyalaraoneela
Contributor III

Hi Sergiosolis,

   I made my module to run as wifi and bluetooth individually, but while running in coexistence mode, on boot bluetooth modules will get inserted and then if I start wifi it is not starting.

Do I need to enable anything in the Android BSP to run coex mode???

Please suggest me how to proceed further??

Platform : IMX6SL.

OS: Android kitkat 4.4.3

Thanks and Regards,

Mutyalarao.

0 件の賞賛
返信