Bitabake fail imx.8quadxplus

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bitabake fail imx.8quadxplus

2,738件の閲覧回数
NajiyaNazrin
Contributor I

I need to display qt creator GUI on i.mx 8quadxplus

i did what exaclty as said in yocto users guide:-

1.install Host packages

 

  • sudo apt-get install gawk wget git-core diffstat unzip texinfo gcc-multilib

  • sudo apt-get install build-essential chrpath socat cpio python python3 python3-pip python3-pexpect

  • sudo apt-get install xz-utils debianutils iputils-ping python3-git python3-jinja2 libegl1-mesa libsdl1.2-dev

  • sudo apt-get install pylint3 xterm rsync curl zstd pzstd lz4c lz4 libssl-dev

 

in case:

E: Unable to locate package pzstd

E: Unable to locate package lz4c

do:

sudo apt update && apt install -y zstd liblz4-tool

sudo apt install zstd

sudo apt-get install zstd lz4

 

 

2.Setting up the Repo utility

 

 

To install the “repo” utility, perform these steps:

1. Create a bin folder in the home directory.

$ mkdir ~/bin (this step may not be needed if the bin folder already exists)

$ curl https://storage.googleapis.com/git-repo-downloads/repo > ~/bin/repo

$ chmod a+x ~/bin/repo

2. Add the following line to the .bashrc file to ensure that the ~/bin folder is in your PATH variable.

$export PATH=~/bin:$PATH

 

3 Yocto Project Setup

 

First, make sure that Git is set up properly with the commands below:

$ git config --global user.name "Your Name"

$ git config --global user.email "Your Email"

$ git config –list

 

then,

$ mkdir imx-yocto-bsp

$ cd imx-yocto-bsp

$ repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-kirkstone -m imx-5.15.52-2.1.0.xml

$ repo sync

XWayland image on i.MX 8QuadXPlus MEK

$ DISTRO=fsl-imx-xwayland MACHINE=imx8qxpmek source imx-setup-release.sh -b build-xwayland

$ bitbake imx-image-full

 

But its showing errors

WARNING: libunistring-native-1.0-r0 do_fetch: Failed to fetch URL https://ftp.gnu.org/gnu/libunistring/libunistring-1.0.tar.gz, attempting MIRRORS if available

WARNING: libtasn1-native-4.18.0-r0 do_fetch: Failed to fetch URL https://ftp.gnu.org/gnu/libtasn1/libtasn1-4.18.0.tar.gz, attempting MIRRORS if available

ERROR: qtbase-native-6.3.2-r0 do_compile: ExecutionError('/home/inntot/imx-yocto-bsp/build-xwayland/tmp/work/x86_64-linux/qtbase-native/6.3.2-r0/temp/run.do_compile.1072662', 1, None, None)

ERROR: Logfile of failure stored in: /home/inntot/imx-yocto-bsp/build-xwayland/tmp/work/x86_64-linux/qtbase-native/6.3.2-r0/temp/log.do_compile.1072662

 

ERROR: Task (virtual:native:/home/inntot/imx-yocto-bsp/sources/meta-qt6/recipes-qt/qt6/qtbase_git.bb:do_compile) failed with exit code '1'

 

0 件の賞賛
返信
3 返答(返信)

2,724件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @NajiyaNazrin 

After installation of the required packages in host machine, One can try to clean the existing yocto build and then re-compile the whole repository. That would be really helpful to resolve all the dependencies.

Thanks & Regards

Sanket Parekh

0 件の賞賛
返信

2,726件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @NajiyaNazrin 

I hope you are doing well.

Can you please share the local.conf file of yocto setup?

Thanks & Regards

Sanket Parekh

0 件の賞賛
返信

2,711件の閲覧回数
NajiyaNazrin
Contributor I

MACHINE ??= 'imx8qxpmek'
DISTRO ?= 'fsl-imx-xwayland'
PACKAGE_CLASSES ?= 'package_rpm'
EXTRA_IMAGE_FEATURES ?= "debug-tweaks"
USER_CLASSES ?= "buildstats"
PATCHRESOLVE = "noop"
BB_DISKMON_DIRS ??= "\
STOPTASKS,${TMPDIR},1G,100K \
STOPTASKS,${DL_DIR},1G,100K \
STOPTASKS,${SSTATE_DIR},1G,100K \
STOPTASKS,/tmp,100M,100K \
HALT,${TMPDIR},100M,1K \
HALT,${DL_DIR},100M,1K \
HALT,${SSTATE_DIR},100M,1K \
HALT,/tmp,10M,1K"
PACKAGECONFIG:append:pn-qemu-system-native = " sdl"
CONF_VERSION = "2"

DL_DIR ?= "${BSPDIR}/downloads/"
ACCEPT_FSL_EULA = "1"

# Switch to Debian packaging and include package-management in the image
PACKAGE_CLASSES = "package_deb"
EXTRA_IMAGE_FEATURES += "package-management"

0 件の賞賛
返信