Best environment for new application

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Best environment for new application

2,052件の閲覧回数
fabio_poiatti
Contributor III

Hi

for IMX.6 processor and for a beginner, which is the best environment to develop new application?

I'm talking about ... development tools, debug, toolchain, bsp ...

I saw the IMXLINUX (I presume from NXP/Frescale) and YOCTO projects ...

I'm a little confused ...

Thanks

Fabio

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

1,936件の閲覧回数
fabio_poiatti
Contributor III

I'm having some problem regarding toolchain for yocto application.

I have the EVK correctly configured with the BSP coming together with the hardware

How can I build a simple application like Hello world?

I'm very confused ...

0 件の賞賛
返信

1,936件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Fabio

one can check nxp software web page giving overview of software and tools for

i.mx development

i.MX Software | NXP 

https://community.nxp.com/docs/DOC-1616 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,936件の閲覧回数
fabio_poiatti
Contributor III

Thanks

I checked both ... but in your opinion which is the best way to imx.6 development (BSP and application

design)?

I mean ... easier ... best support ...

Fabio

0 件の賞賛
返信