Best environment for new application

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Best environment for new application

2,047 Views
fabio_poiatti
Contributor III

Hi

for IMX.6 processor and for a beginner, which is the best environment to develop new application?

I'm talking about ... development tools, debug, toolchain, bsp ...

I saw the IMXLINUX (I presume from NXP/Frescale) and YOCTO projects ...

I'm a little confused ...

Thanks

Fabio

Labels (2)
0 Kudos
Reply
3 Replies

1,931 Views
fabio_poiatti
Contributor III

I'm having some problem regarding toolchain for yocto application.

I have the EVK correctly configured with the BSP coming together with the hardware

How can I build a simple application like Hello world?

I'm very confused ...

0 Kudos
Reply

1,931 Views
igorpadykov
NXP Employee
NXP Employee

Hi Fabio

one can check nxp software web page giving overview of software and tools for

i.mx development

i.MX Software | NXP 

https://community.nxp.com/docs/DOC-1616 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,931 Views
fabio_poiatti
Contributor III

Thanks

I checked both ... but in your opinion which is the best way to imx.6 development (BSP and application

design)?

I mean ... easier ... best support ...

Fabio

0 Kudos
Reply