BUCK2 efficiency of PCA9450A together with i.MX8M Mini

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BUCK2 efficiency of PCA9450A together with i.MX8M Mini

Jump to solution
1,823 Views
lumen
Contributor III

Hi

The PMIC PCA9450A has an input range of 2.85V to 5.5V and has six high efficient step-down regulators. To optimize our power design we would like to know the efficiency of the reference design of the PCA9450A with the i.MX8M Mini depending on the input voltage. Is there an efficiency curve depending on the input voltage and the load current available or do I need to measure it on the evaluation board? For what input voltage is the PCA9450A optimized for low load?

To estimate the efficiency of the PCA9450A BUCK2 theoretically I need also the rise and fall times of the High- and Low-Side FET of the Buck converter. 

Best Regards,

Patrick

Labels (2)
Tags (2)
0 Kudos
Reply
1 Solution
1,775 Views
guoweisun
NXP TechSupport
NXP TechSupport

Please check the typical efficiency curves attached.

View solution in original post

0 Kudos
Reply
2 Replies
1,370 Views
Pavithra31R
Contributor I

1. Can I use the same efficiciency information with i.MX Nano processor as well?

2. If I provide 5V Input to LDO and take 0.85V as output,(This is shown in the compute module schematics) the efficiency is less than 20%. Is it okay to operate LDO in this conditions?

 

0 Kudos
Reply
1,776 Views
guoweisun
NXP TechSupport
NXP TechSupport

Please check the typical efficiency curves attached.

0 Kudos
Reply