BT1120 output

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BT1120 output

2,330 Views
carmilili
Contributor III

Hello everybody,

     Do  you have a patch for IMX6Q  to output "progressive" BT656/1120 now?

     I have saw the link of Patch to Support BT656 and BT1120 Output For i.MX6 BSP.

     But It tell me do not have the patch some times ago.

thank you!

Labels (3)
0 Kudos
Reply
3 Replies

2,084 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hello Carmili,

I think maybe it is a missunderstood, let me attach you the patch for  Linux 3.0.35_4.1.0 based on LTIB.

Added patch for L3.0.35_4.1.0_GA BSP, the file is "L3.0.35_4.1.0_GA_bt656_output_patch_2013-09-30.zip".


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,084 Views
carmilili
Contributor III

I am so happy to see your reply.But the patch is only support interlace BT656/BT1120,the progressive BT1120 do not support.

0 Kudos
Reply

2,084 Views
joanxie
NXP TechSupport
NXP TechSupport

unfortunately, we don't have plan to release patch for BT656/BT1120 progressive mode

0 Kudos
Reply