BSP for sabrelite board.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BSP for sabrelite board.

3,238件の閲覧回数
mutyalaraoneela
Contributor III

Hi all,

  Can you please tell me how to download the Board support package for sabrelite OR where can I get the complete BSP (kernel + u-bbot source + file system) Is there any document that can help me in downloading the same.

Thanks in advance !!!!

ラベル(2)
0 件の賞賛
返信
5 返答(返信)

3,038件の閲覧回数
mutyalaraoneela
Contributor III

Hi Fabio,

    I need to build customized image, I want to enable some features and build my kernel. For that I need kernel source, u-boot source and root file system

Thanks in advance.

0 件の賞賛
返信

3,038件の閲覧回数
gary_bisson
Senior Contributor III

Hi,

If you want to generate the same images as the one provided on our website I suggest you read our blog post:

http://boundarydevices.com/what-is-yocto-and-how-can-i-start/

It describes how to download and build a Yocto image for your board.

Regards,

Gary

0 件の賞賛
返信

3,038件の閲覧回数
BiyongSUN
NXP Employee
NXP Employee
0 件の賞賛
返信

3,038件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

You can check their sources at Boundary Devices · GitHub

Regards,

Fabio Estevam

0 件の賞賛
返信

3,038件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

Have your tried their prebuilt images?

http://boundarydevices.com/imx6-builds/

0 件の賞賛
返信