Automotive support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Automotive support

1,974 Views
PavelM
NXP Employee
NXP Employee

Varroc customer ask for available support for i.MX UL:

  1. Which ASIL level can we achieve with UL?
  2. DO we have partners for Autosar on i.MX6 UL
Labels (1)
1 Reply

1,805 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Pavel,

>> Which ASIL level can we achieve with UL?

On the chip-level we do not support ASIL authentication. But on the i.MX6UL Circuit Modules support customers do the ASIL authentication.

>>DO we have partners for Autocar on i.MX6 UL?

Yes,  there are three ways, the details situation is depending on your product use.

Three ways are as follows:

1. NXP, our i.MX FAE team & AE team

2. The FAE of Distributor

3.IDH
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------