Audio sai2 mclk

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Audio sai2 mclk

5,035件の閲覧回数
jieh朱
Contributor III

Hello, I am using imx6ul, the kernel is linux4.14.78,
I used the i2s external audio chip, but the audio clock is wrong and I can't generate the clock I want. I checked the imx6ul chip manual and found

pastedImage_1.png

pastedImage_6.png

pastedImage_5.png

The register configuration is 10 for PLL4 as the parent clock. But I read it out is 00.
My device tree configures the PLL4 bit parent clock

pastedImage_3.png

pastedImage_4.png

I should do it exclusively?

0 件の賞賛
返信
5 返答(返信)

4,759件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Jiehuai,

   From source code below, we can know the clock outputs on JTAG_TMS PAD:

    pinctrl_sai2: sai2grp {
        fsl,pins = <
            MX6UL_PAD_JTAG_TDI__SAI2_TX_BCLK    0x17088
            MX6UL_PAD_JTAG_TDO__SAI2_TX_SYNC    0x17088
            MX6UL_PAD_JTAG_TRST_B__SAI2_TX_DATA    0x11088
            MX6UL_PAD_JTAG_TCK__SAI2_RX_DATA    0x11088
            MX6UL_PAD_JTAG_TMS__SAI2_MCLK        0x17088
            MX6UL_PAD_SNVS_TAMPER4__GPIO5_IO04    0x17059
        >;
    };

after system booting is done, you can play a music file, then measure the clock on the JTAG_TMS Pin to check if the clock value is what you want.

(系统启动后,播放一个音乐文件,然后用示波器在这个脚上测一下clock的值是否是你希望的12.288MHz, PLL4配置为786432000Hz,它是12288000Hz的整数倍,配置上是对的,输出的clock应该是正确的。所以,请示波器测量一下,看实际结果)

Have a nice day!
BR,

Weidong

0 件の賞賛
返信

4,760件の閲覧回数
jieh朱
Contributor III

thank you for your reply
After I enable the frequency, I start the error.

pastedImage_3.png

pastedImage_1.png

0 件の賞賛
返信

4,760件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hi Jiehuai,

    On i.MX6UL EVK, default I2S port is also SAI2, so you don't need to change source code if you also use the same codec as that of EVK, below is source code in dts:

    pinctrl_i2c2: i2c2grp {
        fsl,pins = <
            MX6UL_PAD_UART5_TX_DATA__I2C2_SCL 0x4001b8b0
            MX6UL_PAD_UART5_RX_DATA__I2C2_SDA 0x4001b8b0
        >;
    };
......

/* Here is sound card , Machine driver will be loaded here */

    sound: sound {
        compatible = "fsl,imx6ul-evk-wm8960",
               "fsl,imx-audio-wm8960";
        model = "wm8960-audio";
        cpu-dai = <&sai2>;
        audio-codec = <&codec>;
        asrc-controller = <&asrc>;
        codec-master;
        gpr = <&gpr 4 0x100000 0x100000>;   /* This is SAI2_MCLK setting in GPR register */
        /*
                 * hp-det = <hp-det-pin hp-det-polarity>;
         * hp-det-pin: JD1 JD2  or JD3
         * hp-det-polarity = 0: hp detect high for headphone
         * hp-det-polarity = 1: hp detect high for speaker
         */
        hp-det = <3 0>;
        hp-det-gpios = <&gpio5 4 0>;
        mic-det-gpios = <&gpio5 4 0>;
        audio-routing =
            "Headphone Jack", "HP_L",
            "Headphone Jack", "HP_R",
            "Ext Spk", "SPK_LP",
            "Ext Spk", "SPK_LN",
            "Ext Spk", "SPK_RP",
            "Ext Spk", "SPK_RN",
            "LINPUT2", "Mic Jack",
            "LINPUT3", "Mic Jack",
            "RINPUT1", "Main MIC",
            "RINPUT2", "Main MIC",
            "Mic Jack", "MICB",
            "Main MIC", "MICB",
            "CPU-Playback", "ASRC-Playback",
            "Playback", "CPU-Playback",
            "ASRC-Capture", "CPU-Capture",
            "CPU-Capture", "Capture";
    };

........

&clks {
    assigned-clocks = <&clks IMX6UL_CLK_PLL4_AUDIO_DIV>;
    assigned-clock-rates = <786432000>;
};

......

&i2c2 {
    clock_frequency = <100000>;
    pinctrl-names = "default";
    pinctrl-0 = <&pinctrl_i2c2>;
    status = "okay";

    codec: wm8960@1a {
        #sound-dai-cells = <0>;
        compatible = "wlf,wm8960";
        reg = <0x1a>;
        wlf,shared-lrclk;
        clocks = <&clks IMX6UL_CLK_SAI2>;
        clock-names = "mclk";
    };

......
    pinctrl_sai2: sai2grp {
        fsl,pins = <
            MX6UL_PAD_JTAG_TDI__SAI2_TX_BCLK    0x17088
            MX6UL_PAD_JTAG_TDO__SAI2_TX_SYNC    0x17088
            MX6UL_PAD_JTAG_TRST_B__SAI2_TX_DATA    0x11088
            MX6UL_PAD_JTAG_TCK__SAI2_RX_DATA    0x11088
            MX6UL_PAD_JTAG_TMS__SAI2_MCLK        0x17088
            MX6UL_PAD_SNVS_TAMPER4__GPIO5_IO04    0x17059
        >;
    };
......

&sai2 {
    pinctrl-names = "default";
    pinctrl-0 = <&pinctrl_sai2>;
    assigned-clocks = <&clks IMX6UL_CLK_SAI2_SEL>,
              <&clks IMX6UL_CLK_SAI2>;
    assigned-clock-parents = <&clks IMX6UL_CLK_PLL4_AUDIO_DIV>;
    assigned-clock-rates = <0>, <12288000>;
    fsl,sai-mclk-direction-output;
    status = "okay";
};

Are you using i.MX6UL EVK to test it?

BR,

Weidong

0 件の賞賛
返信

4,760件の閲覧回数
jieh朱
Contributor III

thank you for your reply

   I look at the clock tree

pastedImage_1.png

according to dts

pastedImage_3.png

sai2 Parent clock is IMX6UL_CLK_PLL4_AUDIO_DIV

0 件の賞賛
返信

4,760件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hi

 

 Are you using i.MX6UL EVK to test it?

weidong

0 件の賞賛
返信