Audio Interface in IMX7ULP with DMA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Audio Interface in IMX7ULP with DMA

1,072 Views
vivekrajpara
Contributor III

Hello,

Setup:

IMX7ULP + dig mic 

Queries

1) Is there a way to capture audio data using DMA over I2S interface? if yes, how much max audio data(at 16k sample rate) can be captured?

2) Is there a way to access I2S interface from Cortex A7 processor? 

Looking forward to a helpful response. It would be great if someone can provide sample applications for audio capturing on IMX7ULP either on M4/A7.

Thanks in advance

Regards,

Vivek

Labels (2)
Tags (2)
0 Kudos
Reply
1 Reply

986 Views
joanxie
NXP TechSupport
NXP TechSupport

1) yes, refer to the schematic, imx7ulp uses wm8960, refer to the driver of wm8960, which can support up to SNDRV_PCM_FORMAT_S24_LE

2) one can set in dts file

imx7ulp.dtsi\dts\boot\arm\arch - linux-imx - i.MX Linux kernel 

for more detailed information, pls refer to the enclose file, focus on the Chapter 7 Audio

 
0 Kudos
Reply