Assistance Required for Booting Linux from eMMC on Custom i.MX8MP Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Assistance Required for Booting Linux from eMMC on Custom i.MX8MP Board

782 Views
sunilaerxlabs
Contributor I

Hi, 

We are currently developing a custom video recorder device based on the i.MX8MP SoC. At present, we are running Linux OS booting from an SD card connected via the SDHC2 interface.

Our next goal is to migrate the boot process to an eMMC device connected to the SDHC3 interface. However, our custom board does not expose a USB-OTG port. As a workaround, we followed the guidance from this post and attempted to flash the eMMC using the dd command.

For this process, we prepared a bootable SD card and connected it to the SoC through a USB-A port using an SD card reader. Unfortunately, when executing the dd command, the system either hangs after copying approximately 150–170 MB of data or enters a kernel panic.

We have attached the relevant kernel logs and screenshots for your reference. We would appreciate your assistance in diagnosing and resolving this issue so that we can successfully boot Linux from the eMMC.

Thank you for your support.

IMX8MP_Getting_Stuck_While_DD.png

0 Kudos
Reply
1 Reply

756 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

I will continue with this inquiry in your submitted support ticket.

Best regards.

0 Kudos
Reply