Ask help for electron application under imx8

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ask help for electron application under imx8

3,251件の閲覧回数
askli1983
Contributor I

Hi,

I develop the vue project, and use the Electron-builder to package it under Linux.
I copy the electron application to the yocto system.
It can’t run well,it give the error ‘Trace/breakpoint trap’.

Do you know imx8 support the electron UI application? How to run it?

Thanks

Huajun

タグ(4)
0 件の賞賛
返信
3 返答(返信)

3,205件の閲覧回数
mgonzalezg9
Contributor II

Having the same problem. In my case electron-builder installs electron 13.0.0 but when the installed app is launched, Segmentation Fault is thrown.

0 件の賞賛
返信

3,241件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Which version you use? You need use electron that support wayland.

0 件の賞賛
返信

3,230件の閲覧回数
askli1983
Contributor I

It is Yocto Zeus,imx6 som chip, could you give some guide about it how to run the electron package application?

0 件の賞賛
返信