[Arrow/i.MX8MN/Linux L5.4.3_1.0.0]TensorFlow lite Acceleration issues

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

[Arrow/i.MX8MN/Linux L5.4.3_1.0.0]TensorFlow lite Acceleration issues

跳至解决方案
2,267 次查看
Lambert
NXP Employee
NXP Employee

 

Project info are below shown:

Software: BSP 5.4.3_1.0.0  (tensorflow + keras)

Hardware: imx8m nano, pico zense Dcam710(USB)

Pls refer to attached for detail.

标签 (1)
0 项奖励
回复
1 解答
2,252 次查看
DevinJiao
NXP Employee
NXP Employee

Hi Lambert,

We don't have optimization for OpenCL in OpenCV. If customer wants to get a better performance, running OpenCV on CPU is a good option.

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,253 次查看
DevinJiao
NXP Employee
NXP Employee

Hi Lambert,

We don't have optimization for OpenCL in OpenCV. If customer wants to get a better performance, running OpenCV on CPU is a good option.

0 项奖励
回复