Application crash with error - EGLFS: OpenGL windows cannot be mixed with others

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Application crash with error - EGLFS: OpenGL windows cannot be mixed with others

5,044 次查看
1182614726
Contributor III

大家好,

            目前使用的imx6solo,BSP为Yocto L4.1.15-2.1.0版本.

            bitbake编译时配置为framebuffer,而不是X11.

            现在需要在QT中显示一个动画,报如下错误:

            

            Application crash with error - EGLFS: OpenGL windows cannot be mixed with others
            请教各位NXP大神协助,谢谢!
标签 (1)
0 项奖励
回复
2 回复数

4,763 次查看
joanxie
NXP TechSupport
NXP TechSupport

this issue isn't imx6 bsp issue, you can refer to the QT forum:

[QTBUG-38405] ComboBox causes crash when using -platform eglfs - Qt Bug Tracker 


Have a great day,
Joan

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

4,763 次查看
1182614726
Contributor III

Hi Joan,

         

            好的,非常感谢

0 项奖励
回复