Any suggestion for embedded Wi-Fi?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Any suggestion for embedded Wi-Fi?

3,093 次查看
MaximeC
Contributor I

Hi everyone,

 

I start a new design with I.MX51.  I'm looking for an embedded Wi-Fi module on my board.

 

I saw the RS9110-N-11-26 from "Redpine signals".  I'm looking for something like that but this one has max 65Mbps.

 

I would like 802.11abgn with 150Mbps max.

 

Any suggestion?

 

Thx, Maxime

标记 (1)
0 项奖励
回复
5 回复数

2,880 次查看
JoeApache
Contributor I

Hey Max,

     As far I read in datasheet of RS9110-N-22-01, which could be your second option, Redpine does not charge for license... The N-22-01 is open firm-ware ready to work.  

0 项奖励
回复

2,880 次查看
MaximeC
Contributor I

I just catch up your answer.

 

The best option we found - so far - is the module RS9110-N-11-03.  We don't want to use a chipset, we prefer to go with a module for a couple of reasons...

 

We are actually dealing with Redpine regarding the expensive annual license for using their products...  I'll let you know.

 

Thanks, Max

0 项奖励
回复

2,880 次查看
MarianoGoluboff
Contributor III

Does it have to be a module? The Redpine Signals RS9116  does 150mbps and has an SDIO interface so it can interface to the i.MX51.

 

http://www.redpinesignals.com/Products/Chipsets/RS9116.html

0 项奖励
回复

2,880 次查看
MaximeC
Contributor I

Thx Rick,

Their max bit rate is 54Mbps.  Thx anyway. 

Max

0 项奖励
回复

2,881 次查看
satank
Contributor I

Not sure what their bit rates are, but check out http://www.wi2wi.com/.

0 项奖励
回复