Any official freescale kernel support real time preempt patch?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Any official freescale kernel support real time preempt patch?

1,676件の閲覧回数
johnmartin
Contributor I

Hello,

In this moment, we are using kernel version 3.18.11 from osadl with real time support. My imx6dl works fine with jitters no more high that 100us, but it doesnt use official kernel from freescale.

My doubt is that official kernel from freescale support preempt real time patch ??

I just tried but when I compile, it has a lot of errors

Any advice?

Best regards.

ラベル(6)
0 件の賞賛
返信
1 返信

1,367件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi John

one can look at rt-patch

https://lists.yoctoproject.org/pipermail/meta-freescale/2015-July/014611.html

https://www.kernel.org/pub/linux/kernel/projects/rt/3.10/older/patch-3.10.17-rt12.patch.bz2

official FSL BSP releases below seems do not support it

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREBRD&fpsp=1&tab=Design_Tool...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信