Any official freescale kernel support real time preempt patch?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Any official freescale kernel support real time preempt patch?

1,650 Views
johnmartin
Contributor I

Hello,

In this moment, we are using kernel version 3.18.11 from osadl with real time support. My imx6dl works fine with jitters no more high that 100us, but it doesnt use official kernel from freescale.

My doubt is that official kernel from freescale support preempt real time patch ??

I just tried but when I compile, it has a lot of errors

Any advice?

Best regards.

Labels (6)
0 Kudos
Reply
1 Reply

1,341 Views
igorpadykov
NXP Employee
NXP Employee

Hi John

one can look at rt-patch

https://lists.yoctoproject.org/pipermail/meta-freescale/2015-July/014611.html

https://www.kernel.org/pub/linux/kernel/projects/rt/3.10/older/patch-3.10.17-rt12.patch.bz2

official FSL BSP releases below seems do not support it

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREBRD&fpsp=1&tab=Design_Tool...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply