Android13 GKI Unknown symbol

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Android13 GKI Unknown symbol

4,448件の閲覧回数
Leo-Ze
Contributor I

Hello,


I'm currently on the imx8mp with Android 13_v1.2.0 and hit a snag with the GKI export symbol failing.

I have integrated an out-of-tree LTE driver, and after referring to the User Guide(included the necessary settings in imx8mp_gki.fragment and ShardBoardConfig.mk).

Additionally, after updating the abi_gki_aarch64_imx & abi_gki_aarch64.xml as per UserGuide section 9.5 and reflashing,I still encounter messages like "Unknown symbol."

imx8mp_LTE.png

 

 

 

 

 

Could you provide a more detailed approach or possible reasons for this error?

Thanks.

 

0 件の賞賛
返信
6 返答(返信)

4,262件の閲覧回数
Leo-Ze
Contributor I

Hi @Zhiming_Liu ,

Is there any update?

--

 

Regards,

Leo Wang

0 件の賞賛
返信

4,250件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @Leo-Ze 

I am downloading the AOSP13 and test refering the Guide

Please refer the steps to update .stg at same time, thanks!

Zhiming_Liu_0-1712623056211.png

 

0 件の賞賛
返信

4,411件の閲覧回数
Leo-Ze
Contributor I

Hi Zhiming,

now I use is android 13 (kernel 5.15), According to user guide...

I think is the same thing(abi_gki_aarch64.xml)?

LeoZe_0-1712126684903.png

If so, then despite updating the abi_gki_aarch_imx and abi_gki_aarch64.xml files

I'm still encountering the "Unknown symbol" issue.

It seems like I might have missed some crucial steps...

Could you please provide a more detailed approach?

Thanks.

--

 

Regards,

Leo Wang

0 件の賞賛
返信

4,416件の閲覧回数
Leo-Ze
Contributor I

Hi Zhiming,

I referenced the following step: Export-new-symbols 

The abi_gki_aarch64_imx and abi_gki_aarch64.xml files have been updated,

abi_gki_aarch64_imx.pngabi_gki_aarch64_xml.png

then I copied the abi_gki_aarch_imx and abi_gki_aarch64.xml files to the NXP kernel directory:

"android_build/vendor/nxp-opensource/kernel_imx/android/"

and after recompiling and flashing, the "Unknown symbol error" still appears during boot-up, as shown in the previous image:

qmi_wwan_q: Unknown symbol netdev_stats_to_stats64
qmi_wwan_q: Unknown symbol arp_create

 

Additionally, I would like to inquire about the step "update abi_gki_aarch64.stg".

What does this step entail? I couldn't find any relevant information in the User Guide.

Thanks.

--

 

Regards,

Leo Wang

0 件の賞賛
返信

4,415件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @Leo-Ze 

 

Please refer this :

Zhiming_Liu_0-1712125570112.png

 

Best Regards

Zhiming

 

0 件の賞賛
返信

4,422件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @Leo-Ze 

Have you finish the 9.4 How to export new symbols? You need update abi_gki_aarch64_imx first and then update abi_gki_aarch64.stg.

 

Zhiming_Liu_0-1712107100676.png

 

Best Regards

Zhiming

0 件の賞賛
返信